Timer

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Timer

5,132 次查看
ernestsnaith
Contributor I
Just playing with timers and they seem increment every two clock cylces, is this right, i thought it was every 4 or maybe 1.
标签 (1)
0 项奖励
回复
3 回复数

1,645 次查看
ernestsnaith
Contributor I

Sorry, its a 9s12xdt512, using low power pierce oscillator at 4MHz. I have set the prescaler to the 128 max and set an LED to flash when the timer is over 0xF000. I was curious to see if i understood the timer so i timed how long the LED cycle took, it turned out to be 4.2 seconds. I thought it should be 1/ 4,000,000(clock) / 65536 (max timer value) all * 128 = 2.1 second

register wise i set TSCR2 to 0x07 and TSCR1 to 0x80

Message Edited by ernestsnaith on 05-02-200603:10 PM

0 项奖励
回复

1,645 次查看
Steve
NXP Employee
NXP Employee

If you have a 4MHz crystal the bus speed (and source of the timer clock) is 2MHz so your maths is correct. If you need the S12X to go faster you should enable the PLL.
You can have a larger prescaler on the timer by using the precision mode (see this thread: http://forums.freescale.com/freescale/board/message?board.id=16BITCOMM&message.id=861)

(Alban created link)

Message Edited by Alban on 05-03-2006 11:10 AM

0 项奖励
回复

1,645 次查看
imajeff
Contributor III
Perhaps you could be more specific if you want to know why. There are registers which control how many bus cycles per increment of TCNT. You could also specify what MCU
0 项奖励
回复