The usage of ADC0 internal channels

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

The usage of ADC0 internal channels

2,389 次查看
jeffcharles
Contributor III

Hi,

We can select the analog input channel of ADC0 about s9s12zvl, the screenshots in the attachment is about the usage of ADC0 internal channels. I try to use the four internal channels, please see my configuration code in the attachment. The result is that:

1. Internal_0 (ADC temperature sensor)      => the adc result is 0x110(272 D)

2. Internal_1(Bandgap Voltage VBG or Chip temperature sensor VHT)      => the adc result is 0x7b(123 D)

3. Internal_4(BATS Vsup sensor voltage)      => the adc result is 0x0

4. Internal_5(High Voltage input Port L0)      => the adc result please see the attachment

My problems are that:

1)  What is the difference between ADC temperature sensor and chip temperature sensor?

2)  I can find the calculation formula about CPMUHTCTL like this:

VHT(temp) = VHT(150) - (150 - temp) * dVHT = 2.4V - (150-temp) * 5.25(typical value) mV/℃

VHT(temp) = 123/1023*5 = 601.17mV

601.17mV = 2400mV - (150 - temp) * 5.25mV/℃

=> temp = -192.63℃

The calculation result is unbelievable, is there anyting wrong with my configuration?

3)  Does the calculation formula applicated for ADC temperature sensor too?

4)  From the result we can see the it does not work about internal_4, does BATS sensor need additional configuration?

5)  You can see the HVI0 test result in the attachment:

The result is accurate in the range of 7V and 23V, but it is almost unchanged over the 23V. It means that in order to ensure the measurement accuracy, the measured voltage should be less than 23V?

Please give me some guide,thanks!

Best regards,

Jeff

1 回复

1,931 次查看
dianabatrlova
NXP TechSupport
NXP TechSupport

Hi,

1.The temperature sensor is an integral part of the on-chip voltage regulator and the ADC temperature sensor is part of ADC module.

2. The typical value of VHT(150) is specified (2.4V), but min and max values are not specified. Therefore, the sensor must be calibrated.

You can refer to AN3624 S12X Temperature Sensor, the sensor on S12Z is the same.
3. Unfortunately, there is no conversion formula for the ADC internal_0 sensor.
4. Regarding BATS, see the attached example
5. The HVI circuit has a standoff voltage. So, the HVI cannot reach the full scale of the ADC
See the case https://community.nxp.com/message/899295

Best regards,

Diana