The difference between S9S12VR48AF0VLC and S9S12VR48AAVLCR

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

The difference between S9S12VR48AF0VLC and S9S12VR48AAVLCR

1,753 Views
GanapatiBhat
Contributor I

Team,

Can someone clarify the difference between S9S12VR48AF0VLC and S9S12VR48AAVLCR. when I decoded the part number the one which is highlighted in red seem to be product revision information. Can you please let me know what is the change.?

Thanks

Ganapati Bhat

 

 

 

 

0 Kudos
Reply
3 Replies

1,695 Views
TOMMY2
Contributor I

一样 易阳易彝雅彝

0 Kudos
Reply

1,731 Views
lama
NXP TechSupport
NXP TechSupport

Hi,

S9S12VR48AF0VLC... F0 is a code for mask set 0N59H which also points to a factory.

- S9S12VR48AF0VLC ... mask set 0N59H
- S9S12VR48AL0VLC ... mask set 0P79C
These two devices are absolutely the same, mask sets are the same but two different factories.


The newer code (the second letter A in S9S12VR48AAVLCR) determines the same mask set but the factory can not be recognized.

So, mask set A = mask set F0(0N59H) = mask set L0(0P79C)
or
S9S12VR48AAVLCR = S9S12VR48AF0VLC = S9S12VR48AL0VLC

The difference is the only in a delivery option where "R" means tape&reel. If there is no "R" then it is Tray.

 

Best regards,

Ladislav

0 Kudos
Reply

1,689 Views
GanapatiBhat
Contributor I

Thanks . This helps

0 Kudos
Reply