Team,
Can someone clarify the difference between S9S12VR48AF0VLC and S9S12VR48AAVLCR. when I decoded the part number the one which is highlighted in red seem to be product revision information. Can you please let me know what is the change.?
Thanks
Ganapati Bhat
一样 易阳易彝雅彝
Hi,
S9S12VR48AF0VLC... F0 is a code for mask set 0N59H which also points to a factory.
- S9S12VR48AF0VLC ... mask set 0N59H
- S9S12VR48AL0VLC ... mask set 0P79C
These two devices are absolutely the same, mask sets are the same but two different factories.
The newer code (the second letter A in S9S12VR48AAVLCR) determines the same mask set but the factory can not be recognized.
So, mask set A = mask set F0(0N59H) = mask set L0(0P79C)
or
S9S12VR48AAVLCR = S9S12VR48AF0VLC = S9S12VR48AL0VLC
The difference is the only in a delivery option where "R" means tape&reel. If there is no "R" then it is Tray.
Best regards,
Ladislav
Thanks . This helps