The LIN stack test log of S12ZVL MCU

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

The LIN stack test log of S12ZVL MCU

ソリューションへジャンプ
1,914件の閲覧回数
dustyko
Contributor II

Hi :

 

I am using FSL LIN 2.x Stack Package 4.5.7 in S12ZVL MCU. 

There is a test log in this LIN 2.x Stack Package  ( please to see the attached file ).


After reviewed this test log , my end customer find a warning in some of test items is as below.

 

Does anyone can explain the following warnings ?  
It seems that is the test equipment limited the capabilities.  

Is it right ?

 

Thanks.

 

 

2.1 3.2 Variation of Length of break field low phase: Passed

 

Test case begin:

2016-05-05 14:41:13

(logging timestamp 8.330741)

Test case end:

2016-05-05 14:41:36

(logging timestamp 31.574407)

Verdict Information

Test case could not be fully executed!

Test Case Sequence

 

Timestamp

Test Step

Description

Result

8.330741

Initialization

Triggering manual IUT HW-reset

-

9.490509

Tester confirmation with 'Yes'.

-

9.510509

Initialization

Due to XL-hardware capabilities this testcase performed with 1 bit time steps instead of required 0.1 bit time steps

warning

 

2.19 3.13.1 Bit rate tolerance, IUT without making use of synchronization. Master deviation from nominal bit rate = + 0.5%: Passed

 

Test case begin:

2016-05-05 14:42:06

(logging timestamp 61.554794)

Test case end:

2016-05-05 14:42:07

(logging timestamp 62.951864)

Verdict Information

Test case could not be fully executed!

Test Case Sequence

 

Timestamp

Test Step

Description

Result

61.554794

Initialization

Triggering manual IUT HW-reset

-

62.801509

Tester confirmation with 'Yes'.

-

62.821509

Execution

Sending ReadByIdentifier (Id=2) with master bit rate = 9600 bps

-

62.821509

Execution

Due to XL-hardware capabilities ReadByIdentifier request in this testcase sent with the nominal master bit rate 9600 bps instead of required 9648 bps

warning

62.836201

Execution

Send ReadByIdentifier request (Id=2, NAD=0x5, SID=0x1E, FID=0x2)

pass

 

Original Attachment has been moved to: CanoeMaster_9600_S122zvl32_9600_autobaud_no.html.zip

0 件の賞賛
返信
1 解決策
1,551件の閲覧回数
RadekS
NXP Employee
NXP Employee

Hi Dusty,
Yes, that is the limitation of the test equipment that we used for Regression Test for porting LIN Stack to support new platforms. The limitation is explained clearly in the description related to “Warning”.

The LIN Stack Package v4.5.7 for S12Z has the Certificate of LIN 2.2A Conformance for Master and Slave Nodes with other qualified test equipment.

I hope it helps you.

Have a great day,
Radek

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,552件の閲覧回数
RadekS
NXP Employee
NXP Employee

Hi Dusty,
Yes, that is the limitation of the test equipment that we used for Regression Test for porting LIN Stack to support new platforms. The limitation is explained clearly in the description related to “Warning”.

The LIN Stack Package v4.5.7 for S12Z has the Certificate of LIN 2.2A Conformance for Master and Slave Nodes with other qualified test equipment.

I hope it helps you.

Have a great day,
Radek

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
1,551件の閲覧回数
dustyko
Contributor II

Hi  Radek :

Thank you for all your assistance !!

I have implemented my LIN functions in S12ZVL MCU based on  LIN Stack Package v4.5.7.

This LIN Stack Package is a powerful tool and easy to use , thanks.

Because my end customer very care this system's reliability. 

We need to provide some of reliability test data , example : ageing parameters , LIN protocol certification report and LIN resynchronization function.

So, may I have some of your comments about the questions is as below :

1.   May I have the certification report about LIN 2.2A conformance ?

2.   Do you have any idea about LIN resynchronization function ?  

      I have got some of information from NXP Application Note : AN3756.

      It seems this function just implemented in some of S08 MCU , I think I need to add this function to S12ZVL MCU.  

Thank you again for everything you're done.

Best Regards,

Dusty Ko

0 件の賞賛
返信