Temperature over I2C???? (Schematics and protocol)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Temperature over I2C???? (Schematics and protocol)

2,786 Views
RChapman
Contributor I
This message contains an entire topic ported from a separate forum. The original message and all replies are in this single message. We have seeded this new forum with selected information that we expect will be of value to you as you search for answers to your questions.
 
Posted: Thu May 19, 2005 6:13 am    
 
Hello!

I have to measure temperatures with my controller. I use a HCS12 MC9S12DJ64 contoller.
One alternative is to measure with the Dallas DS1621 Digital Thermometer over I2C. I´m an absolut newbie Sad and I need your help to configure the protocol and to design the schematics.
Perhaps the I2C protocol is written and I can use it for free?? Wink
I want to program the controller in C with the ICC compiler.
Greetings
Posted: Thu May 19, 2005 7:53 am    
 
If you download the free special edition of codewarrior you can use the "processor expert" to create the init code for the IIC module. Then use either CW or ICC to develop your app.
Posted: Thu May 19, 2005 9:37 am    
 
Sorry, which free special edition do you mean?
I was on the Metrowerks download page. I just found the Developer studio, OSEKturbo and CodeWarrior for Freescale 68HC12/HC(S)12 Encirq Data Expert! I don´t know the right software package.
 
Posted: Thu May 19, 2005 9:48 am    
 
 
Posted: Thu May 19, 2005 10:24 am    
 
Thank you for the link!
I´ve downloaded the software and I will test it soon!
CU
Labels (1)
0 Kudos
Reply
0 Replies