TWR-S12G128 LIN Data Not Receiving

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

TWR-S12G128 LIN Data Not Receiving

ソリューションへジャンプ
1,767件の閲覧回数
Deepak1
Contributor IV

Hi !

I have TWR-S12G128. I am not able to get the LIN Tx data on pin no.2 of COM_EN (Also checked on Pin no. 1). To see the data is receiving or not I have connected Oscilloscope probe to Pin no. 2 of COM_EN and continuously sending data on the LIN bus.

Following settings I have made

1. I have connected LIN Bus to Pin no. 4 of J6. (Pin 1,2,3 are kept open)

2. Pin no. 1-2,3-4 of JP3 LIN_PWR are short.(no slave is connected,no external supply is given).

3. SW6 is ON.

4. All Pins of COM_EN are kept open. (Just want to see data is receiving or not at the pin).

5. PWR_SEL JP5 Pin no. 3-4 are short.

 

Please suggest to get the data.

Thanks !

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
1,674件の閲覧回数
Deepak1
Contributor IV

HI !

Problem Solved. Now I am able to see the data at pin 2 of COM_EN

I have connected +12v at pin 3 & GND at pin 1 of J6 connector. Also the pins 1-2 & 3-4 of JP3 LIN_PWR are short.

Using supply from OSBDM to the board by shorting Pin 3-4 of JP5 PWR_SEL.

As i am thinking the supply from OSBDM will also give supply to LIN Trans receiver.

Thanks for the support !

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,675件の閲覧回数
Deepak1
Contributor IV

HI !

Problem Solved. Now I am able to see the data at pin 2 of COM_EN

I have connected +12v at pin 3 & GND at pin 1 of J6 connector. Also the pins 1-2 & 3-4 of JP3 LIN_PWR are short.

Using supply from OSBDM to the board by shorting Pin 3-4 of JP5 PWR_SEL.

As i am thinking the supply from OSBDM will also give supply to LIN Trans receiver.

Thanks for the support !

0 件の賞賛
返信