TCP/IP

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

TCP/IP

3,514 Views
RChapman
Contributor I
This message contains an entire topic ported from a separate forum. The original message and all replies are in this single message. We have seeded this new forum with selected information that we expect will be of value to you as you search for answers to your questions.
 
Posted: Tue Jul 26, 2005 9:33 am    
 
Hello all,
I need info ( datasheets, manual,example Very Happy ) about TCP/IP.
I want to use hcs12.

thank
 
Posted: Tue Jul 26, 2005 10:36 am    
 
Hello

I know of two free stacks, try and google for UIP or freetcp, i do not have the links here, but UIP is fairly easy to find. If you are going to use MC68HC12NE64 i do have a port of UIP, including a driver for the EPHY and EMAC.
 
Labels (1)
0 Kudos
Reply
1 Reply

1,395 Views
Richly
Contributor III
RChapman wrote:
If you are going to use MC68HC12NE64 i do have a port of UIP, including a driver for the EPHY and EMAC.


Does this port compile using Freescale's CodeWarrior (Special Edition)? If so, how does one go about getting a copy?

I know Pierre Morency ported uIP to the NE64 based on a Gnu development system -- available from <http://www.ericengler.com/downloads/uIP-HCS12NE-release-1.0.zip>. Has anyone ported Morency's version to CodeWarrior?

Thanks,
Richard
0 Kudos
Reply