TCNT not running

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

TCNT not running

3,119件の閲覧回数
Psych0o0
Contributor I

Hi,

 

I'm working with a MC9S12DP256 using TC4 as output compare, but I encounter troubles with the free run counter TCNT. This is how I initialize the timer :

 

// Enable Timer 4 for 1ms clickTIOS        = 0x10; TIE_C4I     = 1;TSCR1_TEN   = 1;TSCR1_TSWAI = 1;TSCR1_TSFRZ = 1;// Run timerTC4 = OS_TIMER_PERIOD;

 

I use CodeWarrior 5.9 under Vista, and TCNT is never incremented, the simulator indicates the value "undefined" for it, whereas it works well at school with CodeWarrior 3.1 under XP...What's the problem ?

 

Regards.

 

Jonathan

ラベル(1)
0 件の賞賛
返信
4 返答(返信)

2,000件の閲覧回数
kef
Specialist I

In true time simulator menu "HCS12 FCS"->"Set Derivative...", try selecting MC9S12DP256B.

 

Also if you used project wizard, included "derivative.h" should contain something like this:

 

#pragma LINK_INFO DERIVATIVE "mc9s12dp256b"

If you don't want to include derivative.h, then try adding above pragma to one of your *.c files.

0 件の賞賛
返信

2,000件の閲覧回数
Psych0o0
Contributor I

I tried to replace the following pragma in "derivative.h" : 

#include <mc9s12dp256.h>#pragma LINK_INFO DERIVATIVE "mc9s12dp256"

by

 

#include <mc9s12dp256.h>#pragma LINK_INFO DERIVATIVE "mc9s12dp256b"

 

and it works ! Thanks for your help !

 

Jonathan.

Message Edited by Psych0o0 on 2009-10-08 11:46 AM
0 件の賞賛
返信

2,000件の閲覧回数
Lundin
Senior Contributor IV
You should post a service request for this so that Freescale fixes it. MC9s12dp256b is a very buggy obsolete silicon mask that you DONT want to use. Remove the "B" and you will get the correct part number.
0 件の賞賛
返信

2,000件の閲覧回数
kef
Specialist I

Then TCNT should run. It works OK for me with all your settings listed above, TCNT advances properly while stepping or running.

 

0 件の賞賛
返信