Strange AxIDE driver problem for MC9S12HY64 demo board

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Strange AxIDE driver problem for MC9S12HY64 demo board

1,127 次查看
KeithO
Contributor I
I can scarcely believe it, but when I went to install the AxIDE utility today for the MC9S12HY64 demo board, it failed at the point where one has to pick the target directory. The default is a directory on the C drive, but in my case since I have a dual boot Linux / XP system, the hard drive is the E: drive instead. I click on the icon to browse for the target folder and the wizard then exits with a message that the C drive is not available. I basically have no opportunity to browse or even edit the C to E drive letter in the path. It is as if the fixed drive is "hard wired" to C drive in the code.... Anyone know a workaround or updated driver utility that does not have this problem ? The executable I am having a problem with is AxIDE385.exe Dated 7/26/2004 9:59am Thanks
标签 (1)
0 项奖励
回复
1 回复

726 次查看
J2MEJediMaster
Specialist I

It sounds like you need to file a Servce Request on that. Click here to submit an on-line service request.

 

---Tom

0 项奖励
回复