Stand-alone BDM flash programmer for HCS12 ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Stand-alone BDM flash programmer for HCS12 ?

3,402 Views
cant
Contributor II
I wish to build a stand-alone Flash programmer using BDM for to program the HCS12 family using a flash card (1GB) for the program code and another flash card for to program a test program in RAM.
Does anyone has already built something similar and can share all the schematics, program code etc. maybe using a 9S12UF32 because it has the memory card interface ?
 
I know that there is a CyclonePro from P&E but it is not exactly what I am looking for.
Thanks a lot
cant66
Labels (1)
0 Kudos
Reply
1 Reply

1,446 Views
imajeff
Contributor III
I've only thought about it. Hope you share with the rest of us when you get it going, since you believe in sharing :smileyhappy:

I think the UF32 would be great for it. I also don't see why you would need two memory cards. Mine would just be one, even If I do need to copy a special file on each one that is loaded into ram for the program.

I think it would be an exellent solution for most small business, if develloped right and open-source.
0 Kudos
Reply