Stall Error occurred

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Stall Error occurred

2,704 Views
jtpark
Contributor IV

Hello,

Using MC9S12ZVML128_BLDC_Sensorless S/W, I tested BLDC motor by own board.

Stall error was occurred when there is load on BLDC motor.

Please refer to the attached.

stall check function is as below.

 

void StallCheck(void)

{

           tU16 max = 0, min = 65535;

 

           if (periodZC_F_PhA>max){

                      max = periodZC_F_PhA;

           }

           if (periodZC_F_PhA<min){

                      min = periodZC_F_PhA;

           }

           if (periodZC_F_PhB>max){

                      max = periodZC_F_PhB;

           }

           if (periodZC_F_PhB<min){

                      min = periodZC_F_PhB;

           }

           if (periodZC_F_PhC>max){

                      max = periodZC_F_PhC;

           }

           if (periodZC_F_PhC<min){

                      min = periodZC_F_PhC;

           }

           if (periodZC_R_PhA>max){

                      max = periodZC_R_PhA;

           }

           if (periodZC_R_PhA<min){

                      min = periodZC_R_PhA;

           }

           if (periodZC_R_PhB>max){

                      max = periodZC_R_PhB;

           }

           if (periodZC_R_PhB<min){

                      min = periodZC_R_PhB;

           }

           if (periodZC_R_PhC>max){

                      max = periodZC_R_PhC;

           }

           if(periodZC_R_PhC<min){

                      min = periodZC_R_PhC;

           }

 

           periodZcAvrg = period6ZC / 6;

 

           if((max > (periodZcAvrg << 1)) || (min < (periodZcAvrg >> 1))){

                      if (stallCheckCounter < STALLCHECK_MAX_ERRORS){

                                  stallCheckCounter++;

                      }

           }else{

                      if (min < STALLCHECK_MIN_CMT_PERIOD){

                                  if (stallCheckCounter < STALLCHECK_MAX_ERRORS){

                                             stallCheckCounter++;

                                  }

                      }else{

                                  if (stallCheckCounter > 0){

                                             stallCheckCounter--;

                                  }

                      }

           }

           if(stallCheckCounter >= STALLCHECK_MAX_ERRORS){

                      StallError = 1;

           }else{

                      StallError = 0;

           }

}

Would you provide solution for this issue?

Thanks.

1 Reply

2,492 Views
pachamatej
NXP Employee
NXP Employee

Hi,

I have a set of questions to be answered before we can work together on the solution:

1) Does your hardware provide enough power to run the motor under load?

2) Does your motor run with the devKit hardware?

3) Have you changed the application settings to accommodate your motor?

4) Does your motor start with no load? 

Thank you,

Regards,

Matej

0 Kudos
Reply