Stall Error occurred

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Stall Error occurred

2,664件の閲覧回数
jtpark
Contributor IV

Hello,

Using MC9S12ZVML128_BLDC_Sensorless S/W, I tested BLDC motor by own board.

Stall error was occurred when there is load on BLDC motor.

Please refer to the attached.

stall check function is as below.

 

void StallCheck(void)

{

           tU16 max = 0, min = 65535;

 

           if (periodZC_F_PhA>max){

                      max = periodZC_F_PhA;

           }

           if (periodZC_F_PhA<min){

                      min = periodZC_F_PhA;

           }

           if (periodZC_F_PhB>max){

                      max = periodZC_F_PhB;

           }

           if (periodZC_F_PhB<min){

                      min = periodZC_F_PhB;

           }

           if (periodZC_F_PhC>max){

                      max = periodZC_F_PhC;

           }

           if (periodZC_F_PhC<min){

                      min = periodZC_F_PhC;

           }

           if (periodZC_R_PhA>max){

                      max = periodZC_R_PhA;

           }

           if (periodZC_R_PhA<min){

                      min = periodZC_R_PhA;

           }

           if (periodZC_R_PhB>max){

                      max = periodZC_R_PhB;

           }

           if (periodZC_R_PhB<min){

                      min = periodZC_R_PhB;

           }

           if (periodZC_R_PhC>max){

                      max = periodZC_R_PhC;

           }

           if(periodZC_R_PhC<min){

                      min = periodZC_R_PhC;

           }

 

           periodZcAvrg = period6ZC / 6;

 

           if((max > (periodZcAvrg << 1)) || (min < (periodZcAvrg >> 1))){

                      if (stallCheckCounter < STALLCHECK_MAX_ERRORS){

                                  stallCheckCounter++;

                      }

           }else{

                      if (min < STALLCHECK_MIN_CMT_PERIOD){

                                  if (stallCheckCounter < STALLCHECK_MAX_ERRORS){

                                             stallCheckCounter++;

                                  }

                      }else{

                                  if (stallCheckCounter > 0){

                                             stallCheckCounter--;

                                  }

                      }

           }

           if(stallCheckCounter >= STALLCHECK_MAX_ERRORS){

                      StallError = 1;

           }else{

                      StallError = 0;

           }

}

Would you provide solution for this issue?

Thanks.

1 返信

2,452件の閲覧回数
pachamatej
NXP Employee
NXP Employee

Hi,

I have a set of questions to be answered before we can work together on the solution:

1) Does your hardware provide enough power to run the motor under load?

2) Does your motor run with the devKit hardware?

3) Have you changed the application settings to accommodate your motor?

4) Does your motor start with no load? 

Thank you,

Regards,

Matej

0 件の賞賛
返信