Some questions about "Function GFLIB_ControllerPIrAW"

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Some questions about "Function GFLIB_ControllerPIrAW"

2,158件の閲覧回数
maxxu
Contributor IV
Hi I'm designing a BLDC driver with Automotive Math and Motor Control Library Set for NXP MC9S12ZVM。 I have a few questions about Function GFLIB_ControllerPIrAW。 1、Are there three functions here, and what is the relationship between them Function GFLIB_ControllerPIrAW Function GFLIB_ControllerPIrAW_F32 Function GFLIB_ControllerPIrAW_F16 2、How to distinguish "differentiation methods"? “Trapezoidal”,“Backward Rect”,“Forward Rect” How to reflect in the code? Which one is used in “S12ZVML-MINIBRD_BLDC_Sensorless_CW_IDE” ? I think it's using the “Forward Rect”,But put the parameters in the formula “ GFLIB_ControllerPIrAW_Eq2” The result is u(k) = u(k-1) + KP*(e(k)-e(k-1)) + KI*Ts*e(k-1), However,The standard formula of discrete PI is u(k) = u(k-1) + KP*(e(k)-e(k-1)) + KI*Ts*e(k), The two formulas are not the same. Is there something wrong with my deduction 3、What is the specific meaning of f32acc and f16inerrk1? f32acc f16inerrk1 There is no detailed description of the document, which I can't understand Hope to get the help of experts, thank you very much!
0 件の賞賛
返信
2 返答(返信)

2,144件の閲覧回数
petrz_
NXP Employee
NXP Employee
0 件の賞賛
返信

2,154件の閲覧回数
maxxu
Contributor IV

Typography error, apply to delete this post

0 件の賞賛
返信