Software guide welcome

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Software guide welcome

1,655件の閲覧回数
LittleBit
Contributor I
We want to implement IP-stack on MC9S12NE64.
I believe there are several strategies:
- use Open TCP/IP stack
- use CMX/Micronet TCP/IP-stack
- use ?

Can somebody help and indicate when to use which IP-stack tool ?

ラベル(1)
0 件の賞賛
返信
1 返信

920件の閲覧回数
mjbcswitzerland
Specialist V
Hi

Look also at the uTasker stack (it includes OS, TCP/IP stack, device drivers are the uTasker simulator running a simulated NE64 in a real network). Online demo at http://demo.uTasker.com (the device it is running on changes and is not necessarily the NE64 but it is single.chip...)

However I also recommend you look at the equivalent Coldfire devices. (eg. M52232 - see overview here: http://www.utasker.com/forum/index.php?topic=256.0) since they are much more powerful, have vastly better peripherals and rather more internal memory (some packages are virtually pin compatible to the NE64) - plus their development support is extremely good. They tend to be cheaper than the NE64 nowadays too so there is really no advantage fo starting a new project with the NE64.

Regards

Mark

www.uTasker.com




0 件の賞賛
返信