Simple question! - MC9S12XEP100

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Simple question! - MC9S12XEP100

1,530 Views
kayji
Contributor I

I just would like to know how fast the system clock is in default setting. Since the crystal oscillator providing frequency to board is only 4MHZ, i just wonder whether real system clock is 4MHZ.

And if it is, anyone know how can use more than 4MHZ, may be 16MHZ clock speed?

Labels (1)
0 Kudos
Reply
1 Reply

1,271 Views
vishaka_maithil
Contributor I

hi dear,

 

If your board has a 4MHz crystal then the bus /clock speed will be 2MHz (for XEP100). If you want 16MHz  clock speed with the same 4MHz crystal , you may use PLL for your application.

0 Kudos
Reply