Showing warning while using ssem and csem function for semaphore lockig and unlocking respectively

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Showing warning while using ssem and csem function for semaphore lockig and unlocking respectively

1,435 次查看
maddularajesh
Contributor III

I defined as follows with MC9S12XEP100 and using main CPU and XGATE.

#define SET_SEMPHR_XGATE(sem_id)   while((!_ssem(sem_id))&&(UI_t)(t1msec-Xgsem_timer)<msec1)){};

#define CLR_SEMPHR_XGATE(sem_id)  _csem(sem_id)

SET_SEMPHR_XGATE(0) 

CLR_SEMPHR_XGATE(0) 

But while compiling with IDE 5.1 it showing as follow warnings

warning: C1801 Implicit parameter declaration for '_ssem'

warning: C1801 Implicit parameter declaration for '_csem'

warning: C1420 Result of function call is ignored  (showing at CLR_SEMPHR_XGATE(0) )

In example programs also _ssem & _csem are not available.

Please provide solution to eliminate all warnings as soon as possible.

Thank you,

Rajesh.

1 回复

1,189 次查看
RadekS
NXP Employee
NXP Employee

Hi Maddula,

You are right, it seems that _csem() and _csem() functions are not implemented in CW files – just defined in intrinsics_xgate.h file.

 

In fact, such functions may be quite redundant since they should do just single assembler commands.

You may use

asm SSEM #sem_id‍

instruction for semaphore locking try.

Additionally, you should check result whether semaphore was locked or not.

Similarly, you may use

asm CSEM #sem_id‍

for semaphore release.

 

Please look at attached simple example code.

 

I hope it helps you.

 

Best regards

Radek