Sharing I/O and External Bus using Processor Expert

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Sharing I/O and External Bus using Processor Expert

3,700 Views
ETCTim
Contributor I
Hello,
I am using the 56F8346 DSP. I want to use A0 thru A10 as the address bus, and then use the remaining A pins as GPIO.
 
Can I set this up in PE? When I turn on the address bus, PE conflicts with the BitIO beans that I setup for the remaining pins. Can I tell PE that I only want to use certain address and data lines for the external bus?
 
Thanks,
Tim
 
Labels (1)
0 Kudos
Reply
2 Replies

1,494 Views
ProcessorExpert
Senior Contributor III
The current version of Processor Expert allows only to enable/disable the whole external bus. However, this feautre has already been implemented into the next upcoming version of Processor Expert.
 
best regards
Petr Hradsky
Processor Expert Support Team
UNIS
0 Kudos
Reply

1,494 Views
imajeff
Contributor III
If it's like the MC9S12, you could only configure the port as GPIO (then bitbang it), or configure the whole port to be an address bus (expanded i/o).
0 Kudos
Reply