Self flash programming of S12DP512

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Self flash programming of S12DP512

1,569 Views
monstor
Contributor II

Dear All,

 

May I know can S12DP512 support self flash programming? E.g. Write data into the 512KBytes program memory.

Labels (1)
Tags (3)
0 Kudos
Reply
1 Reply

1,429 Views
iggi
NXP Employee
NXP Employee

Yes, that is possible.

In order to be able to program/erase all Flash without restriction, the program/erase function must be copied to and executed from a non-flash memory location, RAM or EEPROM for example.

A Flash block cannot be read whilst it is being programmed or erased. Therefore the program and erase function cannot be executed from the flash block which is being operated on.

Here is the application note with the SW example for this specific subject:

Fast NVM Programming for the MC9S12DP256

AN2204SW

Regards,

iggi

0 Kudos
Reply