Self flash programming of S12DP512

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Self flash programming of S12DP512

1,534 次查看
monstor
Contributor II

Dear All,

 

May I know can S12DP512 support self flash programming? E.g. Write data into the 512KBytes program memory.

标签 (1)
标记 (3)
0 项奖励
回复
1 回复

1,394 次查看
iggi
NXP Employee
NXP Employee

Yes, that is possible.

In order to be able to program/erase all Flash without restriction, the program/erase function must be copied to and executed from a non-flash memory location, RAM or EEPROM for example.

A Flash block cannot be read whilst it is being programmed or erased. Therefore the program and erase function cannot be executed from the flash block which is being operated on.

Here is the application note with the SW example for this specific subject:

Fast NVM Programming for the MC9S12DP256

AN2204SW

Regards,

iggi

0 项奖励
回复