STRUCT undefined in XGATE asm

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

STRUCT undefined in XGATE asm

2,017件の閲覧回数
Leojunin
Contributor IV

Hello everyone!! I program in assembler. I'm working on a project where I have a memory structure and the XGATE sees the occupied space but does not identify the variables. How can I explain it? Look at this:

 

COL_CH     STRUCT
TCNT           ds.b   1
DTCYC        ds.b   1
PORT           ds.b   1
MASK          ds.b  1
          ENDSTRUCT

PIXEL         STRUCT
CH_R         TYPE   COL_CH
CH_G         TYPE   COL_CH
CH_B         TYPE   COL_CH
          ENDSTRUCT

COLUMN    STRUCT
LED0         TYPE PIXEL
LED1         TYPE PIXEL
LED2         TYPE PIXEL
LED3         TYPE PIXEL
LED4         TYPE PIXEL
LED5         TYPE PIXEL
LED6         TYPE PIXEL
LED7         TYPE PIXEL
          ENDSTRUCT


DEFAULT_RAM SECTION

ALIGN 2

MyData:
Col0         TYPE COLUMN
Col1         TYPE COLUMN
Col2         TYPE COLUMN
Col3         TYPE COLUMN
Col4         TYPE COLUMN
Col5         TYPE COLUMN
Col6         TYPE COLUMN
Col7         TYPE COLUMN
Col8         TYPE COLUMN
Col9         TYPE COLUMN
ColSlct     ds.b  1

 

If I access "ColSlct" with the XGATE it takes the correct address of "ColSlct" and appears in the data window as defined, but if I try to access for example to "Col0:LED0:CH_R:TCNT" or "Col1:LED0:CH_R:DTCYC" it always points to address 0 and appears in the data window as "undefined"

Why could this be?
If I compile this same structure for the S12X it addresses correctly.

 

I thank you in advance... Is this how it is said?

タグ(5)
0 件の賞賛
返信
2 返答(返信)

1,903件の閲覧回数
Patriciabin
Contributor I

Hello everyone!! I program in assembler. I'm working on a project where I have a memory structure and the XGATE sees the occupied space but ... assembler considers it to be spacebar counter undefined and generates an error message. ... As all other directive in assembler, the directives STRUCT and ... As an example, Infineon uses the Cerberus as standard Debug Port for most of it's devices, e.g. XC16x,. XC2000, TriCore and many others. Defined and defweak symbols use this field as a reference marker. If the field is not NULL, or this structure is the tail of the. undefined symbol list, the ...

 
0 件の賞賛
返信

1,891件の閲覧回数
Leojunin
Contributor IV
I don't understand what you mean or it's incomplete
0 件の賞賛
返信