STOP mode in MC9S12ZVML

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

STOP mode in MC9S12ZVML

ソリューションへジャンプ
3,221件の閲覧回数
xiaofangu
Contributor III

Hello

   My Motor project uses LIN as Communication Bus based on MC9S12ZVML,And I use the IRC to generate the clock.Now,I want to put the micro in stop mode.

   When the MCU enters STOP(I check the ECLK,and there's no frequece), the current is nearly 3mA,so what else may consume the current?

   In addition,Can LIN  wake up the MCU when in stop mode?

   Any help will be appreciated!

Best regards,

xiaofan

0 件の賞賛
返信
1 解決策
2,920件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Hi Xiaofan,

No, the SCI module does not work in Stop mode.

The module wakes up on active edge.  

If the wake-up feature is enabled and if the LIN Bus pin is driven with a dominant level longer than tWUFR followed by a rising edge, the LIN Physical Layer sends a wake-up pulse to the SCI, which requests a wake-up interrupt. (This feature is only available if the LIN Physical Layer is routed to the SCI). (Chapter 19.1.2 of the S12ZVM RM).

Regards,

Daniel

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
2,920件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Hi,

Please see 2N95G and 1N95G errata depending on your device.

e8188 ADC: High current in Stop Mode.

It can be up to 1mA per ADC instance. There is workaround available.

Yes, the LIN PHY can pass wake-up event to SCI module.

Regards,

Daniel

0 件の賞賛
返信
2,920件の閲覧回数
xiaofangu
Contributor III

Hi,Daniel

   Glad to hear  your response.

   I'm still confused,as in full STOP mode,the bus clock is stopped, the sci can still work?

Regards,

   xiaofan.

0 件の賞賛
返信
2,921件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Hi Xiaofan,

No, the SCI module does not work in Stop mode.

The module wakes up on active edge.  

If the wake-up feature is enabled and if the LIN Bus pin is driven with a dominant level longer than tWUFR followed by a rising edge, the LIN Physical Layer sends a wake-up pulse to the SCI, which requests a wake-up interrupt. (This feature is only available if the LIN Physical Layer is routed to the SCI). (Chapter 19.1.2 of the S12ZVM RM).

Regards,

Daniel

0 件の賞賛
返信
2,920件の閲覧回数
xiaofangu
Contributor III

Hello,Daniel

   Thanks for your reply,Now my problem's gone!

Best Regards,

   xiaofan

0 件の賞賛
返信