STAR 12 CPU

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
2,286件の閲覧回数
haricharanreddy
Contributor II

Hi Everyone,

When I am studying the Data sheet of  MC9S12DP256 In the features I came through this

pastedImage_1.png

what Does it mean? what is the difference between Normal CPU and  STAR 12 CPU

Can someone Please explain it?

Thanks in Advance:smileyhappy:

Data Sheet : https://www.nxp.com/docs/en/data-sheet/MC9S12DP256.pdf 

タグ(2)
0 件の賞賛
返信
1 解決策
2,123件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi

Here are some of the mayor differences in between HC12 & HCS12:

HC12                  HCS12
16K-128K        16K-512K
1.2-0.5u             0.25u
8-12MHz            25MHz

Providing smaller dies and updated memory among other changes in our HCS12’s.


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

2 返答(返信)
2,124件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi

Here are some of the mayor differences in between HC12 & HCS12:

HC12                  HCS12
16K-128K        16K-512K
1.2-0.5u             0.25u
8-12MHz            25MHz

Providing smaller dies and updated memory among other changes in our HCS12’s.


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

2,123件の閲覧回数
kef2
Senior Contributor V

Hi,

"normal" was on older HC12 family, MC912D60(A), MC68HC912B32 etc. The biggest difference was top bus clock, HC12 8MHz vs S12 25MHz. A couple of instructions were taking bit more bus cycles.

Edward

0 件の賞賛
返信