SPI loop back with XDT512

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SPI loop back with XDT512

1,837 Views
MAC_HI
Contributor I
Hi iam working with XDT512 ,
 
SPI0 is master and SPI1 is slave
i want to loop back and send the data back to SPI0. 2BYTE data
Any application notes avaiable .please send to me immediately.
is there any internal loop back facility avaiable or i have to connect externally.???
 
Regards
MC
Labels (1)
0 Kudos
Reply
1 Reply

1,169 Views
Alban
Senior Contributor II
Hello,
 
There is no internal loopback between this 2 modules. You will have to put connections externally. No need to cross-over with SPI.
 
What does the Application Note you want would show ?
 
Alban.
0 Kudos
Reply