SCI0 without LIN interface

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

SCI0 without LIN interface

跳至解决方案
10,732 次查看
lotfi_bensalem
Contributor I

Hi,


I use the DEVKIT-S12VR64: Dev Board for #S12VR64 MCU and the CW V5.1. I would like to use a pure serial interface SCI0  without through the LIN interface. At first, I used the serial SCI1 as presented in the LAB3_SCI_S12VR, just to familiarize myself and be sure that the control settings are correct, everything works fine. Then I wanted to adapt this example for the SCI0 interface, but it does not work. In the MC9S12VRRM, it explains on page 82/83 that SCI0 is shared with LINPHY interface. I programmed the register MODRR2 = 0b0110 to use PS1 / TXD0 and PS0 / RXD0 but it does not work. I also tried MODRR2 = 0b1110 to use PT1 / TXD0 and PT0 / RXD0, does not work . Here is a registry initialization code:

//route SCI0
/* MODRR2: MODRR23=0,MODRR22=1,MODRR21=1,MODRR20=0, */ //Module Routing Register 2
setReg8Bits(MODRR2, 0x06U); //TXD0 on PS1, RXD0 on PS0, see page 82, 83
/* LPCR: LPE=0 */ //LIN Control Register (LPCR)
clrReg8Bits(LPCR, 0x08U); //The LIN Physical Layer is in shutdown mode, see page 82, 83
/* PPSS: PPSS1=1,PPSS0=1 */ //polarity select, pull down
setReg8Bits(PPSS, 0x03U);
/* PERS: PERS1=1,PERS0=1 */ //polarity enabled
setReg8Bits(PERS, 0x03U);
/* WOMS: WOMS1=0 */ //Output Wired mode: Push pull
clrReg8Bits(WOMS, 0x02U);

What's wrong ? 

0 项奖励
回复
1 解答
2,513 次查看
dianabatrlova
NXP TechSupport
NXP TechSupport

Hi,

I would like to point to the example code for the S12VR64 MCU where can be seen the initialization, settings, and interrupts of the SCI0. There SCI0 is routed to Port S.

Please refer to the attachment.

I hope it helps you. If you have any questions, let me know.

Best Regards,

Diana

在原帖中查看解决方案

0 项奖励
回复
2 回复数
2,514 次查看
dianabatrlova
NXP TechSupport
NXP TechSupport

Hi,

I would like to point to the example code for the S12VR64 MCU where can be seen the initialization, settings, and interrupts of the SCI0. There SCI0 is routed to Port S.

Please refer to the attachment.

I hope it helps you. If you have any questions, let me know.

Best Regards,

Diana

0 项奖励
回复
2,513 次查看
lotfi_bensalem
Contributor I

Hi Diana,
Thank you for this example, it works well, it allowed me to debug my program and find the problem.
thanks again
Lotfi

0 项奖励
回复