SCI0 without LIN interface

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SCI0 without LIN interface

ソリューションへジャンプ
10,776件の閲覧回数
lotfi_bensalem
Contributor I

Hi,


I use the DEVKIT-S12VR64: Dev Board for #S12VR64 MCU and the CW V5.1. I would like to use a pure serial interface SCI0  without through the LIN interface. At first, I used the serial SCI1 as presented in the LAB3_SCI_S12VR, just to familiarize myself and be sure that the control settings are correct, everything works fine. Then I wanted to adapt this example for the SCI0 interface, but it does not work. In the MC9S12VRRM, it explains on page 82/83 that SCI0 is shared with LINPHY interface. I programmed the register MODRR2 = 0b0110 to use PS1 / TXD0 and PS0 / RXD0 but it does not work. I also tried MODRR2 = 0b1110 to use PT1 / TXD0 and PT0 / RXD0, does not work . Here is a registry initialization code:

//route SCI0
/* MODRR2: MODRR23=0,MODRR22=1,MODRR21=1,MODRR20=0, */ //Module Routing Register 2
setReg8Bits(MODRR2, 0x06U); //TXD0 on PS1, RXD0 on PS0, see page 82, 83
/* LPCR: LPE=0 */ //LIN Control Register (LPCR)
clrReg8Bits(LPCR, 0x08U); //The LIN Physical Layer is in shutdown mode, see page 82, 83
/* PPSS: PPSS1=1,PPSS0=1 */ //polarity select, pull down
setReg8Bits(PPSS, 0x03U);
/* PERS: PERS1=1,PERS0=1 */ //polarity enabled
setReg8Bits(PERS, 0x03U);
/* WOMS: WOMS1=0 */ //Output Wired mode: Push pull
clrReg8Bits(WOMS, 0x02U);

What's wrong ? 

0 件の賞賛
返信
1 解決策
2,557件の閲覧回数
dianabatrlova
NXP TechSupport
NXP TechSupport

Hi,

I would like to point to the example code for the S12VR64 MCU where can be seen the initialization, settings, and interrupts of the SCI0. There SCI0 is routed to Port S.

Please refer to the attachment.

I hope it helps you. If you have any questions, let me know.

Best Regards,

Diana

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,558件の閲覧回数
dianabatrlova
NXP TechSupport
NXP TechSupport

Hi,

I would like to point to the example code for the S12VR64 MCU where can be seen the initialization, settings, and interrupts of the SCI0. There SCI0 is routed to Port S.

Please refer to the attachment.

I hope it helps you. If you have any questions, let me know.

Best Regards,

Diana

0 件の賞賛
返信
2,557件の閲覧回数
lotfi_bensalem
Contributor I

Hi Diana,
Thank you for this example, it works well, it allowed me to debug my program and find the problem.
thanks again
Lotfi

0 件の賞賛
返信