SCI interrupt

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SCI interrupt

3,471 Views
khumphri
NXP Employee
NXP Employee

This message contains an entire topic ported from a separate forum. The original message and all replies are in this single message. We have seeded this new forum with selected information that we expect will be of value to you as you search for answers to your questions.

 

Posted: Thu Dec 29, 2005 10:16am

 

Hi,

 

I'm using the 68hcs12c64 processor and having the following problem with its SCI module:

 

Whenever I receive a Uart signal (checked on a scope) at the SCI interface, the SCI interrupt is asserted. But the Transmit interrupt flag is asserted instead of the Receive interrupt flag, with the transmit interrupt disabled.

 

Does anyone have an idea of what may be happening.

 

Thanks and regards,

 


 

Posted: Thu Dec 29, 2005 10:49am

 

> I'm using the 68hcs12c64 processor and having the

> following problem with its SCI module:

>

> Whenever I receive a Uart signal (checked on a scope)

> at the SCI interface, the SCI interrupt is asserted.

> But the Transmit interrupt flag is asserted instead of

> the Receive interrupt flag, with the transmit

> interrupt disabled.

>

> Does anyone have an idea of what may be happening.

 

Yes. With the little information you gave, I can say that something is probably wrong with your source code.

 

Specifically I can say that the tx interrupt should be asserted as you say it is, unless it is currently sending a character also. Anyway, that's why you sould not enable tx irq until you have data to send.

 


 

Posted: Thu Dec 29, 2005 11:53am

 

> Whenever I receive a Uart signal (checked on a scope)

> at the SCI interface, the SCI interrupt is asserted.

> But the Transmit interrupt flag is asserted instead of

> the Receive interrupt flag, with the transmit

> interrupt disabled.

 

I am not sure about the receive interrupt, but the transmit interrupt flag is set because the transmitter is empty. This flag indicates the status of the transmitter, whether the transmit interript is enabled or not.

 

Regards,

 


 

Posted: Thu Dec 29, 2005 1:53pm

 

Yes, I forgot this detail, otherwise we would not be able to perform polling over Tx flag. Fortunately I found out the problem: another issue of Code Warrior's PE: it looses information of the status flag after reading it.

 

Thanks

Labels (1)
0 Kudos
Reply
0 Replies