S9S12VR48AF0VLF Marking information

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S9S12VR48AF0VLF Marking information

5,261件の閲覧回数
RobertChan
Contributor I

Hi,

 

I have a question about the marking of S9S12VR48AF0VLF.

 

I noticed the final letter of marking can be different

 

Could you help to advise what the marking information stand for?

 

Attached picture for your reference.

 

Thank you.

 

 

 

0 件の賞賛
返信
4 返答(返信)

5,207件の閲覧回数
RobertChan
Contributor I

Hi Lama,

 

Noted.

 

Is it normal that chips with two different marking are mixed in one tray?

 

Best Regards,

Robert

0 件の賞賛
返信

5,242件の閲覧回数
lama
NXP TechSupport
NXP TechSupport

Hi,

The CTLROH a CTLROG are valid trace codes for S9S12VR48AF0VLF.

 

This is an official  MATERIAL MARKING FORMAT of this device

(F)S912                       

VR48AV

MMMMM

ALYWZ

                 

The problem is space on the MCU and a new transformation code for S9S devices which added letters into a part number. The F0 means the mask set 0N59H. The size of package and packing type is clear from physical existence of delivery so the only important value to mention is a temperature range. Moreover, there is only 48 LQFP package produced.

It looks like production decided to use change from S9S12VR48AF0VLF to S912VR48AV and next line for mask set 0N59H. Finally it is the same device even "confusing" numbers are printed if you are not familiar with background. This is not first time they decided to do such compression because of printing and manufacturing possibilities and internal standards.

Best regards,

Ladislav

0 件の賞賛
返信

5,239件の閲覧回数
RobertChan
Contributor I
Hi Ladislav, Noted, one more question, CTLROH and CTLROG , what does the final letter stand for? BR, Robert
0 件の賞賛
返信

5,232件の閲覧回数
lama
NXP TechSupport
NXP TechSupport

Hi,

I am sorry this is internal information.

Best regards,

Ladislav

0 件の賞賛
返信