S12zvl aclk clock deafault value

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S12zvl aclk clock deafault value

1,080 Views
charudattaingal
Contributor IV

Dear all,

 

I want to know the ACLK clock default value in  S12zvl controller to calculate watchdog timer time out.

Labels (1)
0 Kudos
Reply
1 Reply

948 Views
RadekS
NXP Employee
NXP Employee

Hi,

Nominal value of ACLK is 20kHz.

ACLK frequency is divided by 2 when ACLK is selected as clock source for watchdog:

ACLK.png

So, 10kHz is source clock frequency for COP watchdog.

Minimum timeout (CPMUCOP_CR=0x01, CPMUCLKS _COPOSCSEL1=1) is 2^7*(1/10kHz)=12,8ms

Maximum timeout (CPMUCOP_CR=0x07, CPMUCLKS _COPOSCSEL1=1) is 2^17*(1/10kHz)= 13,1072s

Note: ACLK frequency could be trimmed by modifying CPMUACLKTR register value. Note: After reset a value is automatically loaded again from the Flash memory.


I hope it helps you.

Have a great day,
RadekS

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply