S12g family flashing issue using hiwave

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S12g family flashing issue using hiwave

Jump to solution
2,111 Views
inside_system
Contributor II

how to flash S19 file in  S12G family controller using direct flashing tool other than Hiwave coz it doesent work

1 Solution
1,738 Views
lama
NXP TechSupport
NXP TechSupport

Hi,

If you use SW 5.1 (does not work under Windows 10) then download a service pack from our web. Here is the procedure:

https://community.nxp.com/videos/5109   There are also service pack for G64(G48) placed here.

 

If you use CW 5.2 (works under Windows 10) then the procedure is described at:

https://community.nxp.com/message/877065?commentID=877065#comment-877065

 

Note 1; There is no problem if you use as a target device S12G64 for programming of S12G48. They have the same memory map and mask set.

 

Note 2; If you want to only program the device then evaluation version of the CodeWarrior is enough for this purpose. There are no limitations for this task.

 

Best regards,

Ladislav

View solution in original post

4 Replies
1,739 Views
lama
NXP TechSupport
NXP TechSupport

Hi,

If you use SW 5.1 (does not work under Windows 10) then download a service pack from our web. Here is the procedure:

https://community.nxp.com/videos/5109   There are also service pack for G64(G48) placed here.

 

If you use CW 5.2 (works under Windows 10) then the procedure is described at:

https://community.nxp.com/message/877065?commentID=877065#comment-877065

 

Note 1; There is no problem if you use as a target device S12G64 for programming of S12G48. They have the same memory map and mask set.

 

Note 2; If you want to only program the device then evaluation version of the CodeWarrior is enough for this purpose. There are no limitations for this task.

 

Best regards,

Ladislav

1,738 Views
inside_system
Contributor II

Thanks lama... this link  and youtube video solved my problem thank you very much

0 Kudos
Reply
1,738 Views
lama
NXP TechSupport
NXP TechSupport

Hi,
Sorry for later response. The issue appeared in our box just a few minutes ago.

 I have tested it and there is no issue. Could you please check with my procedure?

- Open Hiwave.exe

- Option Target (for example HC12Multilink CyclonePro, 4th option from the left)->Select Derivative

- If the device is secured you can also unsecure. For this purpose you can also download Unsecure12 application from pemicro.com pages.

- Option (Target, for example HC12Multilink CyclonePro)->Connect

- Option (Target, for example HC12Multilink CyclonePro)->Command Files
pastedImage_3.png

    My cmd directory in application

       pastedImage_4.png

- Option File->Load Application
                 Load Code-loads the code only

     pastedImage_5.png

 

- If it still does not work you can use prog12z from www.pemicro.com.    PROG12Z. http://tinyurl.com/l6zrps

Best regards,

Ladislav

0 Kudos
Reply
1,738 Views
inside_system
Contributor II

hello lama,

my Microcontroller S12G48  is not there in target setting, what to do i have codewarrior 5.2 ??

0 Kudos
Reply