S12g family flashing issue using hiwave

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

S12g family flashing issue using hiwave

跳至解决方案
2,106 次查看
inside_system
Contributor II

how to flash S19 file in  S12G family controller using direct flashing tool other than Hiwave coz it doesent work

1 解答
1,733 次查看
lama
NXP TechSupport
NXP TechSupport

Hi,

If you use SW 5.1 (does not work under Windows 10) then download a service pack from our web. Here is the procedure:

https://community.nxp.com/videos/5109   There are also service pack for G64(G48) placed here.

 

If you use CW 5.2 (works under Windows 10) then the procedure is described at:

https://community.nxp.com/message/877065?commentID=877065#comment-877065

 

Note 1; There is no problem if you use as a target device S12G64 for programming of S12G48. They have the same memory map and mask set.

 

Note 2; If you want to only program the device then evaluation version of the CodeWarrior is enough for this purpose. There are no limitations for this task.

 

Best regards,

Ladislav

在原帖中查看解决方案

4 回复数
1,734 次查看
lama
NXP TechSupport
NXP TechSupport

Hi,

If you use SW 5.1 (does not work under Windows 10) then download a service pack from our web. Here is the procedure:

https://community.nxp.com/videos/5109   There are also service pack for G64(G48) placed here.

 

If you use CW 5.2 (works under Windows 10) then the procedure is described at:

https://community.nxp.com/message/877065?commentID=877065#comment-877065

 

Note 1; There is no problem if you use as a target device S12G64 for programming of S12G48. They have the same memory map and mask set.

 

Note 2; If you want to only program the device then evaluation version of the CodeWarrior is enough for this purpose. There are no limitations for this task.

 

Best regards,

Ladislav

1,733 次查看
inside_system
Contributor II

Thanks lama... this link  and youtube video solved my problem thank you very much

0 项奖励
回复
1,733 次查看
lama
NXP TechSupport
NXP TechSupport

Hi,
Sorry for later response. The issue appeared in our box just a few minutes ago.

 I have tested it and there is no issue. Could you please check with my procedure?

- Open Hiwave.exe

- Option Target (for example HC12Multilink CyclonePro, 4th option from the left)->Select Derivative

- If the device is secured you can also unsecure. For this purpose you can also download Unsecure12 application from pemicro.com pages.

- Option (Target, for example HC12Multilink CyclonePro)->Connect

- Option (Target, for example HC12Multilink CyclonePro)->Command Files
pastedImage_3.png

    My cmd directory in application

       pastedImage_4.png

- Option File->Load Application
                 Load Code-loads the code only

     pastedImage_5.png

 

- If it still does not work you can use prog12z from www.pemicro.com.    PROG12Z. http://tinyurl.com/l6zrps

Best regards,

Ladislav

0 项奖励
回复
1,733 次查看
inside_system
Contributor II

hello lama,

my Microcontroller S12G48  is not there in target setting, what to do i have codewarrior 5.2 ??

0 项奖励
回复