S12ZVM current capability w/ complementary darlington

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S12ZVM current capability w/ complementary darlington

Jump to solution
4,242 Views
keisukeninomiya
NXP Employee
NXP Employee

Hello

 

S12ZVM has a capabillity to increase current from 70mA to 170mA with ballast transistor.

Now Customer is asking to increast this current more than 170mA such 300mA.

I think if complementary darlington circuit can achieve this request.

The circuit is one reference as the folloiwng URL.

Let me know if there is possibility or not.

 

Regards,

Nino

 

https://www.google.co.jp/search?q=darlington+transistor&biw=1195&bih=602&tbm=isch&imgil=zOW0z_J42rtR...

Labels (1)
1 Solution
4,021 Views
Wlodek_D_
Senior Contributor II

Hello,

Yes, if there is 300mA required, then your Customer can use PNP Darlington transistor e.g. MJD117 or MMBTA63LT1G from ON Semi (see http://www.onsemi.com/pub_link/Collateral/MJD112-D.PDF or http://www.onsemi.com/pub_link/Collateral/MMBTA63LT1-D.PDF respectively.

It will be safer for MCU to drive Darlington than single transistor with quite low hfe.

Best Regards,

Wlodek_D.

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
5 Replies
4,021 Views
iggi
NXP Employee
NXP Employee

The complementary transistor can be a solution, but per my opinion it is unnecessary.

For example, the max. collector current of BCP53 transistor is 1.5Amps!

http://www.onsemi.com/pub_link/Collateral/BCP53T1-D.PDF

But, if the ballast transistor can supply more than 1A of current, it does not mean we can connect external loads to the MCU pins which will consume such current.

In this case, the user must ensure that the maximum junction temperature is not exceeded. It depends on ambient temperature, thermal package characteristics and MCU power dissipation.

MCU power has to be calculated for the particular application.This is explained in S12ZVM RM, Appendix A.1.7.

Regards,

iggi

0 Kudos
Reply
4,021 Views
keisukeninomiya
NXP Employee
NXP Employee

Hi iggi

Thank you for your feedback.

I have considered your idea with BCP53 PNP transistor.

If customer want to 300mA, regarding Fig2 in BCP53 datasheet, hfe is about 50. Then Ib=Ic/hfe=6mA

Injection current in CCS RM shows 2.5mA for each pins. Then this might be out of spec.

Am I correct ?

Regards,

Nino

0 Kudos
Reply
4,022 Views
Wlodek_D_
Senior Contributor II

Hello,

Yes, if there is 300mA required, then your Customer can use PNP Darlington transistor e.g. MJD117 or MMBTA63LT1G from ON Semi (see http://www.onsemi.com/pub_link/Collateral/MJD112-D.PDF or http://www.onsemi.com/pub_link/Collateral/MMBTA63LT1-D.PDF respectively.

It will be safer for MCU to drive Darlington than single transistor with quite low hfe.

Best Regards,

Wlodek_D.

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
4,021 Views
keisukeninomiya
NXP Employee
NXP Employee

Hi Wlodek

Thanks.

Understood.

Regards,

Nino

0 Kudos
Reply
4,021 Views
jrrlopez
NXP Employee
NXP Employee

Hi Nino,

An additional very important item is the power dissipation considerations for the pass transistor and make sure you don't exceed the maximum power and operating temperature range. For example, if you consider a maximum voltage of 18V and considering the ballast transistor regulates down to 5V with a current demand of 300mA, you are reaching a power dissipation of 3.9W!! (18V - 5V)*0.3 which could be way beyond the power dissipation capabilities of the transistor.

Regards,

Juan