S12ZVM CAN Driver

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S12ZVM CAN Driver

1,756 Views
yanwangwkbj
Contributor I

Hello!  I´m looking for a can driver for the S12ZVM microcontroller! Including CAN TX and RX.Can anybody help me? I´ve searched the net but couldn´t find one!  Thank you very much in advance!

Tags (1)
0 Kudos
Reply
2 Replies

1,570 Views
RadekS
NXP Employee
NXP Employee

Hi Yan,

You may also use the more complex MSCAN S12 driver for your reference.

Note: This driver was created for older S12(X) devices (the CW5 projects cannot be used directly), but the CAN module is still the same.

I hope it helps you.

Have a great day,
Radek

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,570 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hello,

There is an application note:

Using MSCAN on the MagniV® Family (AN4975),

Software: AN4975SW.zip

Regards,

Daniel

0 Kudos
Reply