S12ZVL enable debugging in Full stop mode

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S12ZVL enable debugging in Full stop mode

1,368 Views
charu
Contributor I

Hi Team,

I have put the S12VL micro in Full stop mode using Stop instruction, after executing stop instruction loosing the debugger control.

Currently I am using PE debugger, let me know how to keep BDM mode active after execution of Stop instruction.

Thanks & Regards,

Charudatta

0 Kudos
Reply
1 Reply

1,355 Views
dianabatrlova
NXP TechSupport
NXP TechSupport

Hello,

 

After our discussion in a support ticket I would like to add some points here:

If you need to verify that you are in Full stop mode you can check the Bus clock. Since the Bus clock is stopped in Full-Stop mode, you can monitor the bus clock as ECLK provided ECLKCTL[NECLK] = 0.

In Full-Stop Mode the external oscillator and the oscillator clock monitor are disabled and unfortunately, I didn't find a way to debug the code by PE multilink interface in the Full-Stop Mode.

However, after MCU is awake from stop mode, you can go to Debug Configuration and select "Attach" as debug session type and click on "Debug".

Best regards,

Diana

 

 

Best regards,

Diana

0 Kudos
Reply