S12ZVL SCI Driver

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S12ZVL SCI Driver

Jump to solution
3,881 Views
charudattaingal
Contributor IV

Requesting basic Uart(SCI) driver example code for S12ZVL Micro.

Labels (1)
1 Solution
3,090 Views
RadekS
NXP Employee
NXP Employee

Hi Charudatta,

I prepared for you simple SCI example code for S12ZVL.

Please look at attached project.


I hope it helps you.

Have a great day,
RadekS

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

2 Replies
3,090 Views
lama
NXP TechSupport
NXP TechSupport

Hi,

I would like only to add.

As an SCI debug console you can use FreeMASTER.

The tool is free and you can use different connections between PC and MCU. (UART, BDM, CAN,...)

The tool provides access to the MCU during run mode, provides you  data visualization, recorder and.....

FreeMASTER Run-Time Debugging Tool|NXP 

Best regards,

Ladislav

0 Kudos
Reply
3,091 Views
RadekS
NXP Employee
NXP Employee

Hi Charudatta,

I prepared for you simple SCI example code for S12ZVL.

Please look at attached project.


I hope it helps you.

Have a great day,
RadekS

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------