S12ZVL LIN ldf file configuration

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

S12ZVL LIN ldf file configuration

2,525 次查看
b51447
NXP Employee
NXP Employee

Hi, 

Can we use .ldf GUI editor to configure the "Signal_encoding_types" and "Signal_representation" parts?

i can't find it in GUI editor sheet, however, there are some codes of  "Signal_encoding_types" and "Signal_representation" in the text editor sheet.

Thanks in advance.

标签 (1)
0 项奖励
回复
3 回复数

2,064 次查看
RadekS
NXP Employee
NXP Employee

Hi Remi,

The the "Signal_encoding_types" and "Signal_representation" provide additional information that does not change the behavior of the LIN cluster but provide hints for a presentation of the traffic by bus.

The GUI editor does not parse information in this section.

So users can’t use GUI editor to configure this section.

I hope it helps you.

Have a great day,
Radek

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

2,064 次查看
b51447
NXP Employee
NXP Employee

Hi, Radek,

Thanks for your answer. If customer want to add the information of these two parts. Could we add the information in the text editor window by ourselves? it is available?

0 项奖励
回复

2,064 次查看
RadekS
NXP Employee
NXP Employee

Hi Remi,

Yes, the information in these two parts may be / should be modified by a customer in the text editor.

I hope it helps you.

Have a great day,
Radek

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复