S12ZVC SCI

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S12ZVC SCI

3,503件の閲覧回数
marslin
Contributor I

There are 2 SCI in 12ZVC(48pin). I assign RXD0/TXD0 but can not assign another RXD1/TXD1.

圖片1.png

ラベル(1)
タグ(1)
7 返答(返信)

3,092件の閲覧回数
aaronlee
Contributor V

Hi,

Why does my manual only 1 SCI on S12ZVCA(48-pin)?

pastedImage_2.png

Best Regards,

Aaron

0 件の賞賛
返信

3,092件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Hi Aaron,

You are referring to an outdated version of the RM.

pastedImage_1.png

Regards,

Daniel

3,092件の閲覧回数
aaronlee
Contributor V

Hi Daniel,

It's a good news. Thank you.

Best Regards,

Aaron

0 件の賞賛
返信

3,092件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Hi,

Did you routed SCI1 to the port (SCI1RR)?

Regards,

Daniel

0 件の賞賛
返信

3,092件の閲覧回数
marslin
Contributor I

Daniel ,

I mean I can't  assign the SCI1 via CodeWarrior Development Studio. There is no SCI1 can be selected.

456.png

0 件の賞賛
返信

3,092件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Hi,

I had to edit this answer, because I cannot asign the SCI1 either on S12ZVC 48-pin package.

The problem has been reported, it should be fixed.

I must have checked 64-pin version instead.

Sorry for the misleading information.

Regards,

Daniel

0 件の賞賛
返信

3,092件の閲覧回数
RadekS
NXP Employee
NXP Employee

Hi Mars,

The SCI1 at PT0, PT1 pins have the highest priority. So, there should not be any problem with different functions assigned to these pins.

 

I suppose that issue may be in the code for writing to the MODRR0 register.

This register may be written just once in normal mode. Therefore, you must write complete configuration in a single command.

Correct approach:

MODRR0 = 0x30;‍

Wrong approach:

MODRR0_SCI0 = 1;
MODRR0_SCI1 = 1;
//…‍‍‍

I hope it helps you.

Have a great day,
Radek

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------