S12ZVC Port S Pins Drive Strength

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S12ZVC Port S Pins Drive Strength

1,569件の閲覧回数
amit_dhand
Contributor III

Hello,

 

I want to know the S12ZVC Microcontroller (48 Pin) Port S drive strength. That means how much current it can withstand, especially for PS0, PS1, PS2, PS3.

 

I couldn't find the information in MC9S12ZVCRM_V1_3 document.

 

Like how it is shown for Port P on Page 43 in the above document.

PP0, PP4, PP5 & PP6 supports 25 mA driver strength to VSSX

PP2 supports 20 mA driver strength from VDDX (EVDD)

 

 

Thank you

ラベル(1)
0 件の賞賛
返信
1 返信

1,375件の閲覧回数
RadekS
NXP Employee
NXP Employee

Hi Amit,

Instantaneous maximum current on PP0,PP4,PP5 & PP6 is -30..+80mA

Instantaneous maximum current on PP2 is -70..+25mA

Instantaneous maximum current on all other digital IO pins is -25..+25mA

Pins PP0, PP2, PP4, PP5, PP6 are high current pins with specific characteristics. See Table A-8. 5V I/O Characteristics.

All other digital IO pins are characterized by maximum voltage drop 0.8V with 4mA input/output current. This characteristic is guaranteed across operational conditions and temperature range.

If current load will be higher than 4mA, voltage characteristic could be influenced (voltage drop could be higher).

More details about GPIO structure and behavior could be found in our application note:

AN2434 Input-Output Pin Drivers on HCS12 Family MCUs

http://www.freescale.com/files/microcontrollers/doc/app_note/AN2434.pdf

Note: this application note was created for older S12 families built on 250nm technology. Therefore numbers and some details will not fit, however general information are still valid.


I hope it helps you.


Have a great day,
RadekS


-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信