S12ZVC ADC Power consumption in STOP Mode

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S12ZVC ADC Power consumption in STOP Mode

1,591件の閲覧回数
allenyu
Contributor II

Dear Sirs,

When I tested the S12ZVC MCU's STOP Mode current, If my application has to use AD_MeasureChan (), the STOP Mode current will be too large, about 1mA. Once my application does not use AD_MeasureChan (), the STOP Mode current will be normal, about 45uA. What is the reason for this situation?

ラベル(1)
0 件の賞賛
返信
1 返信

1,309件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Hello Allen,

The ADC can take a higher current in Stop Mode (500μA increasing over time to about 1mA
per ADC instance) if the ADC is enabled and conversions have been done.

Please see S12ZVC_0N23N, Mask Set Errata for Mask 0N23N.

There is a software workaround available.

Regards,

Daniel

0 件の賞賛
返信