S12ZVC ADC Power consumption in STOP Mode

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S12ZVC ADC Power consumption in STOP Mode

1,613 Views
allenyu
Contributor II

Dear Sirs,

When I tested the S12ZVC MCU's STOP Mode current, If my application has to use AD_MeasureChan (), the STOP Mode current will be too large, about 1mA. Once my application does not use AD_MeasureChan (), the STOP Mode current will be normal, about 45uA. What is the reason for this situation?

Labels (1)
0 Kudos
Reply
1 Reply

1,331 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hello Allen,

The ADC can take a higher current in Stop Mode (500μA increasing over time to about 1mA
per ADC instance) if the ADC is enabled and conversions have been done.

Please see S12ZVC_0N23N, Mask Set Errata for Mask 0N23N.

There is a software workaround available.

Regards,

Daniel

0 Kudos
Reply