S12ZVC ADC 12bits Resolution with Processor Expert

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S12ZVC ADC 12bits Resolution with Processor Expert

Jump to solution
2,550 Views
jinliangsun
Contributor III

I'm working with DEVKIT-S12ZVC board. I use processor expert to configure the ADC module. With PE I can only select  8 bits or 10 bits mode but not 12 bits mode. But according to the reference manual it does support 12 bits mode.

1.4.13 Analog-to-Digital Converter Module (ADC)
• 12-bit resolution
• Up to 16 external channels and 8 internal channels
• Left or right aligned result data

...

Is it possible to use 12 bits mode with Processor Expert generated code? 

Thanks,

Bruce

0 Kudos
Reply
1 Solution
2,341 Views
kef2
Senior Contributor V

Hi,

9S12ZVC - 10bit ADC, 9S12ZVCA - 12bit ADC. Did you select non -A derivative?

Edward

View solution in original post

0 Kudos
Reply
3 Replies
2,341 Views
dianabatrlova
NXP TechSupport
NXP TechSupport

Hi jinliangsun,

The Edward is right. When you creating the project you need to choose the variant of MCU S12ZVCA192 (in the case you are using DEVKIT-S12ZVC development platform for S12ZVC|NXP) as you can see below:

pastedImage_53.png

After that, you can select 12bit ADC.

I hope it helps you and thanks, Edward.

Best regards,

Diana

2,340 Views
jinliangsun
Contributor III

Hi Diana,

Thanks for your response. I did select the wrong derivarative.

Regards,

Bruce

0 Kudos
Reply
2,342 Views
kef2
Senior Contributor V

Hi,

9S12ZVC - 10bit ADC, 9S12ZVCA - 12bit ADC. Did you select non -A derivative?

Edward

0 Kudos
Reply