S12ZVC ADC 12bits Resolution with Processor Expert

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S12ZVC ADC 12bits Resolution with Processor Expert

ソリューションへジャンプ
2,531件の閲覧回数
jinliangsun
Contributor III

I'm working with DEVKIT-S12ZVC board. I use processor expert to configure the ADC module. With PE I can only select  8 bits or 10 bits mode but not 12 bits mode. But according to the reference manual it does support 12 bits mode.

1.4.13 Analog-to-Digital Converter Module (ADC)
• 12-bit resolution
• Up to 16 external channels and 8 internal channels
• Left or right aligned result data

...

Is it possible to use 12 bits mode with Processor Expert generated code? 

Thanks,

Bruce

0 件の賞賛
返信
1 解決策
2,322件の閲覧回数
kef2
Senior Contributor V

Hi,

9S12ZVC - 10bit ADC, 9S12ZVCA - 12bit ADC. Did you select non -A derivative?

Edward

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
2,322件の閲覧回数
dianabatrlova
NXP TechSupport
NXP TechSupport

Hi jinliangsun,

The Edward is right. When you creating the project you need to choose the variant of MCU S12ZVCA192 (in the case you are using DEVKIT-S12ZVC development platform for S12ZVC|NXP) as you can see below:

pastedImage_53.png

After that, you can select 12bit ADC.

I hope it helps you and thanks, Edward.

Best regards,

Diana

2,321件の閲覧回数
jinliangsun
Contributor III

Hi Diana,

Thanks for your response. I did select the wrong derivarative.

Regards,

Bruce

0 件の賞賛
返信
2,323件の閲覧回数
kef2
Senior Contributor V

Hi,

9S12ZVC - 10bit ADC, 9S12ZVCA - 12bit ADC. Did you select non -A derivative?

Edward

0 件の賞賛
返信