Hi,
My group met a problem that some of our controllers using S12ZVC failed to boot. The defective rate is about 0.1%。
The phenomenons list as below:
1、turn on the battery, the LDO chip normally sends out VCC 15V while the S12ZVC doesn't boot. VDDX pin on BDM interface is 5V, which is generated from the external PNP controlled by the BCTL pin. Reset pin on BDM is 0.2V.
2、Then, plug in the universal multilink debugger, the S12ZVC boot for a uncertain period of time, sometimes several seconds and sometimes several minutes.
3、Connecting a 4.7k resistor to pull up the reset pin externally doesn't solve the problem.
Since the status is not stable, it is not able to check the registers in debugging mode on the IDE.
Any suggestions to find out what has happened to the chip?
Thank you!