S12XE Interrupt Rising and Falling Edges

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S12XE Interrupt Rising and Falling Edges

ソリューションへジャンプ
1,459件の閲覧回数
rayhall
Contributor V

I  have eight signals on external pins (Port) and I want an interrupt on both rising and falling edges. I cannot find a way to do this. There are options for rising or falling, but not both ?

 

I do not want to capture or record the edges time periods. I just want an interrupt so I can add my own code related to the state of these eight pins.

 

Ray.

ラベル(1)
0 件の賞賛
返信
1 解決策
1,304件の閲覧回数
kef2
Senior Contributor V

TIM and ECT pins, input capture can be configured to interrupt on any edge.

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,304件の閲覧回数
kef2
Senior Contributor V

TIM and ECT pins, input capture can be configured to interrupt on any edge.

0 件の賞賛
返信