S12XE Interrupt Rising and Falling Edges

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S12XE Interrupt Rising and Falling Edges

Jump to solution
1,415 Views
rayhall
Contributor V

I  have eight signals on external pins (Port) and I want an interrupt on both rising and falling edges. I cannot find a way to do this. There are options for rising or falling, but not both ?

 

I do not want to capture or record the edges time periods. I just want an interrupt so I can add my own code related to the state of these eight pins.

 

Ray.

Labels (1)
0 Kudos
Reply
1 Solution
1,260 Views
kef2
Senior Contributor V

TIM and ECT pins, input capture can be configured to interrupt on any edge.

View solution in original post

0 Kudos
Reply
1 Reply
1,261 Views
kef2
Senior Contributor V

TIM and ECT pins, input capture can be configured to interrupt on any edge.

0 Kudos
Reply