S12XE Four Cylinder Engine Management

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S12XE Four Cylinder Engine Management

1,365 Views
rayhall
Contributor V

I am going to develop a engine management ECU based on the S12XE. I have bought the KIT33812ECUEVME Small Engine Control and have studied the code. This has been helpful.

 

I am looking to another code example that will give me a deeper understanding of how to achieve the best engine control.

 

  Ray.

Labels (1)
0 Kudos
Reply
3 Replies

1,252 Views
iggi
NXP Employee
NXP Employee

Hi Ray,

i found a project based on S12P device for a scooter which has a two-cylinder engine i suppose.

Not sure if this can be of help to you, but the actual problem i see if we can share this with you at all.

Maybe it would work with some NDA.

Regards,

iggi

0 Kudos
Reply

1,252 Views
rayhall
Contributor V

Hello Iggi,

Is this the project from the freescale Small Engine Control  KIT33812ECUEVME. If it is, then I have that code as I bought the kit. If not,  then I would be intrested in seeing the code. Maybe email it to me if posible,

Ray.

0 Kudos
Reply

1,252 Views
iggi
NXP Employee
NXP Employee

The project i found (under different name) is the same as KIT912S812ECUEVM_Project.zip delivered with the kit. I compared the source files and there is no difference.

It looks like there are no other codes/projects related with this kit for studying.

Regards,

iggi

0 Kudos
Reply