S12XDP512 PLL Circuit

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S12XDP512 PLL Circuit

1,766 Views
sfb
Contributor I
Hi,
If I don't use PLL how should I connect the VDDPLL, VSSPLL, XFC pins. (Connect them to ground or 5V with resistor or nothing...)
Labels (1)
0 Kudos
Reply
1 Reply

795 Views
DPB
NXP Employee
NXP Employee
The VDDPLL, VSSPLL power domain is required for the oscillator input even if you are not using the PLL.
A decoupling capacitor (220 nF, X7R ceramic) should be placed between these supply lines, the internal voltage regulator supplies the power.

If PLL usage is not required, the XFC pin must be tied to VDDPLL.
0 Kudos
Reply