S12XDP512 PLL Circuit

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

S12XDP512 PLL Circuit

1,741 次查看
sfb
Contributor I
Hi,
If I don't use PLL how should I connect the VDDPLL, VSSPLL, XFC pins. (Connect them to ground or 5V with resistor or nothing...)
标签 (1)
0 项奖励
回复
1 回复

770 次查看
DPB
NXP Employee
NXP Employee
The VDDPLL, VSSPLL power domain is required for the oscillator input even if you are not using the PLL.
A decoupling capacitor (220 nF, X7R ceramic) should be placed between these supply lines, the internal voltage regulator supplies the power.

If PLL usage is not required, the XFC pin must be tied to VDDPLL.
0 项奖励
回复