S12X Flash write access

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S12X Flash write access

4,773 Views
mark99
Contributor I

I implemented the flash routines for the S12 and it works fine.

 

Now I have a new project with HCS12XEP and have to adapt the flash routines. Is it correct that I can write to a flash block while code fetching from a different flash block? Or is it the same like S12 (flash routines in RAM and no IRQ while flash access)? I didn't find an answer in the datasheet.

 

Thanks!

Mark

Labels (1)
0 Kudos
Reply
10 Replies

4,162 Views
kef
Specialist I

Yes, you should disable interrupts and run code from memory, which is readable and not from which you are erasing/programming. Those MCU's, which don't require disable of  interrupts or running from RAM, have CPU halted while flash is being erased or programmed. Yes, you may run from one flash block (block is not the same like page), while other is being programmed.

0 Kudos
Reply

4,162 Views
mark99
Contributor I

Thanks for your answer!

 

I have an other question: I'm trying to write to Flash page E0. What I have to define in prm?

NO_INIT?

 

.prm:

SEGMENTS

      PAGE_E0     = NO_INIT     DATA_FAR IBCC_FAR  0xE08000 TO 0xE0BFFF;

:

PLACEMENT

      NON_VOLATILE_STORAGE    INTO  PAGE_E0;

 

Flash.c:

#pragma CONST_SEG NON_VOLATILE_STORAGE

const char __far non_volatile_data[] = { 0xFFFF };

#pragma CONST_SEG DEFAULT

 

Thank you!

Mark

0 Kudos
Reply

4,162 Views
kef
Specialist I

Either NO_INIT or READ_ONLY. READ_ONLY for settings defined in your code, and implicit zeros for not initialized settings. NO_INIT for not initialized data.

I'm using NO_INIT, because READ_ONLY makes all data reset with data from S-records file, when upgrading firmware using bootloader. I think that old settings should survive firmware upgrade.

 

0 Kudos
Reply

4,162 Views
mark99
Contributor I

Thanks for your help!

 

I actually have a very strange problem. If I run my flash write routine in debug mode (single step), it works. In normal mode (continue) the write access fails with ACCERR=1. Seems I have to look for the error for a while...

 

Mark

0 Kudos
Reply

4,162 Views
mark99
Contributor I

That code (HCS12XDP512) runs in debug mode (single step) fine but not in contiues mode. Any idea where the error could be? Thanks a lot!

 

 

#pragma CODE_SEG .data

 

static void LaunchCommand(void)

{

    // launch flash command

    FSTAT_CBEIF = 1;

 

    // wait for command completion    

    do

    {

    } while (!FSTAT_CCIF);

}

 

#pragma CODE_SEG NON_BANKED

 

    :

    :

    UInt16 *pDestination = (UInt16 *)0x8000;

    PPAGE = 0xE0;

 

    FSTAT = 0x32;                               // clear error flags

    *pDestination = *pSource;              // write data to address    

    FCMD = 0x20;                                // program command    

 

    __asm SEI;                                     // disable interrupts

    LaunchCommand();                        // call routine in RAM

    __asm CLI;                                     // enable interrupts

 

    pSource++;    

    pDestination++;    

    :

 

#pragma CODE_SEG DEFAULT

0 Kudos
Reply

4,162 Views
kef
Specialist I

Hm, should work. But are you running it really on S12XD and not on S12XE?

 

FSTAT_CBEIF = 1; 

 

^^ it shouldn't cause your problem, but this code is clearing not just CBEIF, but also all other FSTAT flags. You know it, right?

 

 

0 Kudos
Reply

4,162 Views
mark99
Contributor I

I'm running on S12XD right now because I only have such a hardware. Later in the project we'll change to S12XE. That means I have to chage my flash routines again right? :smileywink:

 

The problem of the flash write access in continues mode was no code problem. It was a problem of the debugger not refreshed the memory data properly. :smileysad:

 

 

> FSTAT_CBEIF = 1;

> ^^ it shouldn't cause your

> problem, but this code is

> clearing not just CBEIF,

> but also all other FSTAT

> flags. You know it, right?

 

I don't understand...what I have to change...?

 

Thank you very much for your help!

Mark

0 Kudos
Reply

4,162 Views
kef
Specialist I

Right, S12XE has different type of flash and requires different program/erase routines. But this doesn't happen too often. From ancient HC12 until now this is only 4th or so version of flash.

 

Regarding debugger. It doesn't update read only memories, unless you edit memory mapping in debugger to refresh memory when halting. See in P&E Multilnk menu in debugger.

 

> FSTAT_CBEIF = 1;

 

Ok. Let consider more dangerous line:

 

   FSTAT_PVIOL = 1;

 

Looks like innocent attempt to clear PVIOL flag. But in fact this is an attempt to clear all FSTAT flags, including CBEIF! You are launching flash command here. Don't you see how? The answer is in how C bitfields (see how FSTAT_PVIOL is defined in headers) are working. PVIOL bit like other bitfields members not addresseable. You can address only whole bytes, belonging to bitfield struct. So how you or compiler can change just one bit? Only reading whole byte, manipulating read bit pattern, then writing resulting bitpattern back to byte in memory. This is exactly what happens in our example. FSTAT is read with PVIOL set or not, but with CBEIF most likely set. Whatever you do to PVIOL bit in read bit pattern, all other bits are preserved, including CBEIF=1. So you get a write of one to CBEIF, which is an attempt to launch flash command. :smileyhappy:

What to do? Don't use bitfields with flags. Below red lines are wrong. Use green lines

 

FSTAT   |= FSTAT_PVIOL_MASK;  // clears all FSTAT flags

FSTAT   &= ~FSTAT_PVIOL_MASK; // clears all FSTAT flags except PVIOL

FSTAT_PVIOL = 1; // clears all FSTAT flags

FSTAT_PVIOL = 0; // clears all FSTAT flags except PVIOL

FSTAT   =  FSTAT_PVIOL_MASK;

FSTAT  &= FSTAT_PVIOL_MASK; // note no ~

0 Kudos
Reply

4,162 Views
mark99
Contributor I

> FSTAT_PVIOL = 1;

 

Ups, yes I understand the problem of this line. Thank you for you explanations!

 

I'll change

 

FSTAT_CBEIF = 1;

 

to

 

FSTAT = FSTAT_CBEIF_MASK;

0 Kudos
Reply

4,162 Views
mark99
Contributor I

...I did find out it myself: It is possible to read from a Flash block while a command is executing on a different Flash block. :smileywink:

0 Kudos
Reply