S12X Chip Selects

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S12X Chip Selects

3,165 Views
mcgeeph
Contributor II
I'm looking at using the 9S12XDP512CAG.  While working out the connections for all of my peripherals, I realize that I'll need to make use of the IIC that is mux'd with CS0 & CS2.  My concern is, will this hamper my ability to use external RAM?  I've been looking through the datasheet and from what I can tell so far, it doesn't look like there should be any issues.  Though I would just like to make sure that neither chip select is special.  Thanks.
Labels (1)
0 Kudos
Reply
3 Replies

1,887 Views
Steve
NXP Employee
NXP Employee
It depends on what you intend to do with the RAM.
CS0 maps to the "program space" of the MCU so memories controlled with this chip-select are usually extensions to the internal flash and are accessed through PPAGE.
CS2 maps to "extra EEPROM" and external space so access would be via EPAGE or GPAGE
 
Obviously if you intend to place the RAM in those spaces then the loss of the chip selects would make life more complicated. If you plan to place the RAM as an extension to the internal RAM then CS3 is the obvious choice.
The chip-selects are enabled under software control so if you don't need them then don't use them.
Have a look at AN2708 for an explanation on the low level operation of the interface.
0 Kudos
Reply

1,887 Views
mcgeeph
Contributor II

Thank you Steve. 

I was planning on using the RAM as an extention of the internal RAM.  Where is there a listing of specific functions for the different chip selects?  I must have missed that when I was looking. 

0 Kudos
Reply

1,887 Views
Steve
NXP Employee
NXP Employee
Have a look at the global memory map you'll see that the chip select ranges slot neatly into certain memory areas (XDP512 Data Sheet memory map section). This doesn't limit their use but it does indicate where they are most suited. The software implementation will usually be more straightforward if you use the chip selects as indicated.
0 Kudos
Reply